Problem in licesing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem in licesing

1,269件の閲覧回数
VinothLC
Contributor I

When i run the code warrior development suite which is of  FLOATING subscription, after installing the license file, it tells some error with the license file carrying the status as ' Unable to find key from

Win32_PLUGINS_PPCCPU_NOT FIND THE HOST' .

 

It also says waiting for background operation.

 

Please provide help in this.

 

Thanks,

 

Vinoth

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,126件の閲覧回数
J2MEJediMaster
Specialist I

A couple of questions:

 

1) Is the FLEXlm licensing software set up properly on the server? For more information, go to this web page and follow the Vendor Daemons link.

 

2) The licensing software comunicates on certain TCP ports in order to function. This requires that these ports be open (unblocked). Your network administrator needs to ensure that the firewall is not blocking these ports.

 

3) Even though your network adminstrator says the ports are unblocked, insist that he do it. Nine out of ten floating-license problems, from my experience, are because to these critical ports being blocked, even though the IT person says that they aren't. The licensing software can generate a log that can help you spot problems with the network.

 

---Tom

0 件の賞賛
返信