PowerQUICC II Pro MPC8349E-MDS Linux BSP Anyone?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PowerQUICC II Pro MPC8349E-MDS Linux BSP Anyone?

3,498 Views
DaveHawkins
Contributor I
Hi all, I just submitted the following to support, and their automated response suggested to also ask the question here ... so here goes: I have tried on numerous occassions to download the 8349E-MDS BSP CD-ROM ISO (from the Code Warrior Linux BSPs page), CWB-MPC8349E-MDS-LTIB, however the download takes many hours (on a fast T1 connection!), and when complete the ISO image is partially corrupted (or download fails, as it has several times this morning). I've mounted the downloaded ISO on the loopback device under Linux and each time during the BSP install procedure, install fails with a complaint about an Input/Output error (I used the loopback, just to confirm this wasn't a CD burner issue). I need to start working with this board ASAP, and need to update the U-Boot version and kernel versions so that I have source that I can then build and link test programs and device drivers with. If anyone reading the forum has successfully downloaded a copy of the ISO, can you please put it on an FTP site (temporarily anyway), so that I can try downloading the image with a more reliable tool than a browser. Thanks! Dave
Labels (1)
0 Kudos
Reply
2 Replies

1,725 Views
J2MEJediMaster
Specialist I
Send me an e-mail (Tom.Thompson at Freescale.com), with the exact file name you need.

---Tom
0 Kudos
Reply

1,725 Views
DaveHawkins
Contributor I
Hi Tom, thanks for the offer, I've sent you an email.

Dave
0 Kudos
Reply