No. This is not my case.
I have three projects with the different size. I compiled two of them anew in the new version of the CodeWarrior. But during loading a code the window "Could not set PC Entry Point" is sometimes shown and process comes to the end.
Now I try to load "
Phytec dBug environment" into Flash memory which allows to load a code through Ethernet. But this is unsuccessfully with my astable connection.In addition. My EVB: phyCORE-MCF548x.
- Alexey.
Thanks for your help.
I have downloaded CodeWarrior Version 6.2 . However now I have other problem. Connection with the device "USB ColdFire Multilink Rev C" is astable, the window "Couldn not set Entry Point" is frequently shown,
therefore it is difficult to work with the evaluation module.Please, help me.
- Alexey