PlugIn License for CW Special Edition?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

PlugIn License for CW Special Edition?

2,392件の閲覧回数
admin
Specialist II

Halo,

 

i have the MCF52235EVB and CW Special Edition. The CW Special Edition have a 128KB Codesize limit and 32 files per target limit. My Project have less than 32 files an only 40 KB Codesize, but the IDE shows me the following error when i try to compile:

 

Error : Unable to use the plugin "Metrowerks C/C++". It is licensed and a valid license key was not found.

 

Invalid host

 

The hostid of this system does not match the hostid

 

specified in the license file

 

Feature: Win32_ColdFire_Compiler

 

Hostid: 00300585e7d9

 

License path: C:\Programme\Freescale\CodeWarrior for ColdFire V6.3 -

 

\license.dat

 

FLEXlm error: -9,57

 

For further information, refer to the FLEXlm End User Manual,

 

available at "www.macrovision.com

 

What can i do to compile my project?

 

THX

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,038件の閲覧回数
J2MEJediMaster
Specialist I
The error message is stating that the ID value associated with the machine doesn't match what's in the license file. Simply put, CW is rejecting the license. Usually this happens when you move CW to another computer, or reformat the computer's hard drive.

---Tom
0 件の賞賛
返信