P1020RDB NOR FLASH PROGRAMMING

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

P1020RDB NOR FLASH PROGRAMMING

17,108件の閲覧回数
Nuevo
Contributor I

Hi

I am trying to Re-Flash the NOR-FLASH...... using the codewarrior 10.3.3 and i have followed the following steps

Window > Show View > Other--->Debug-->Target Task-->ok

then imported the P1020RDB_NOR FLASH.xml file

I didnt change the s29gl128p base address

then I added the the vsc2bin file using Add program/verify action from add action. Here i selected the Erase sectors  before program and verify after program --> then i set the address offset value as FF7FE000,---> add program action

then I added the the u-boot_nor.bin file using Add program/verify action from add action. Here i selected the Erase sectors  before program and verify after program --> then i set the address offset value as FFF80000,---> add program action

then i excute it

 

fl::target -lc "FLASH-core00_RAM_P1020_Download"

fl::target -b 0x2000 0x30000

fl::target -v on -l off

cmdwin::fl::device -d "S29GL128P" -o "8Mx16x1" -a 0xff000000 0xffffffff

cmdwin::fl::image -f "C:\\Freescale\\BSP image\\P1020RDB_Images\\P1020RDB\\Pre_Build_images\\vsc2bin" -t "Binary/Raw Format" -re off -oe on -o 0xff7fe000

cmdwin::fl::erase image

Beginning Operation ...  

-------------------------

Performing target initialization ...  

Downloading Flash Device Driver ... 

Reading flash ID ...

Erasing Sector 0xFF7E0000 to 0xFF7FFFFF 

Erasing ...

Erase Command Succeeded  

cmdwin::fl::write verify

Beginning Operation ...  

-------------------------

Programming file C:\Freescale\BSP image\P1020RDB_Images\P1020RDB\Pre_Build_images\vsc2bin 

Downloading Flash Device Driver ... 

Reading flash ID ...

Downloading 0x00001FF8 bytes to be programmed at 0xFF7FE000 

Executing program with verify .... 

Program with Verify Command Succeeded  

cmdwin::fl::image -f "C:\\Freescale\\BSP image\\P1020RDB_Images\\P1020RDB\\Pre_Build_images\\u-boot_nor.bin" -t "Binary/Raw Format" -re off -oe on -o 0xfff80000

cmdwin::fl::erase image

Beginning Operation ...  

-------------------------

Downloading Flash Device Driver ... 

Reading flash ID ...

Erasing Sector 0xFFF80000 to 0xFFF9FFFF 

Erasing Sector 0xFFFA0000 to 0xFFFBFFFF 

Erasing Sector 0xFFFC0000 to 0xFFFDFFFF 

Erasing Sector 0xFFFE0000 to 0xFFFFFFFF 

Erasing .....

Erase Command Succeeded  

cmdwin::fl::write verify

-------------------------

Programming file C:\Freescale\BSP image\P1020RDB_Images\P1020RDB\Pre_Build_images\u-boot_nor.bin 

Downloading Flash Device Driver ... 

Reading flash ID ...

Downloading 0x00010000 bytes to be programmed at 0xFFF80000 

Downloading 0x00010000 bytes to be programmed at 0xFFF90000 

Executing program with verify .... 

Program with Verify Command Succeeded  

Downloading 0x00010000 bytes to be programmed at 0xFFFA0000 

Downloading 0x00010000 bytes to be programmed at 0xFFFB0000 

Executing program with verify .... 

Program with Verify Command Succeeded  

Downloading 0x00010000 bytes to be programmed at 0xFFFC0000 

Downloading 0x00010000 bytes to be programmed at 0xFFFD0000 

Executing program with verify .... 

Executing program with verify ..... 

Program with Verify Command Succeeded  

Downloading 0x00010000 bytes to be programmed at 0xFFFE0000 

Downloading 0x00010000 bytes to be programmed at 0xFFFF0000 

Executing program with verify .... 

Program with Verify Command Succeeded  

 

But our board is not bring-up some junk data is show in flash.....

Please can u help me how to solve this problem......

ラベル(1)
0 件の賞賛
返信
34 返答(返信)

3,490件の閲覧回数
addiyi
NXP Employee
NXP Employee

More question for you:

1. When you power on or reset the board, in terminal are displayed that characters?

2. What about your board, it is p1020rbd or p1020rdb-pc?

3. Also, I wander why your board is connected on COM4, do you have 4 COM ports on your PC? Or how is the connection between your PC and board?

4. Do you use an adapter from UART0 (RJ45 connector) to serial and then a serial cable to your PC?

Adrian

0 件の賞賛
返信

3,490件の閲覧回数
Nuevo
Contributor I

Hi

serial cable is connected between pc and target board is proper...i used 115200 baud rate only......

0 件の賞賛
返信

3,490件の閲覧回数
addiyi
NXP Employee
NXP Employee

Please provide switch setup of your board.

Adrian

0 件の賞賛
返信

3,490件の閲覧回数
Nuevo
Contributor I

1. When you power on or reset the board, in terminal are displayed that characters     === yes

2. What about your board, it is p1020rbd or p1020rdb-pc === p1020rdb-pc

3. Also, I wander why your board is connected on COM4, do you have 4 COM ports on your PC? Or how is the connection between your PC and board

4. Do you use an adapter from UART0 (RJ45 connector) to serial and then a serial cable to your PC?  == i used rj45 connector one end is connecting to UART0 another end is connection to UART TO USB Connector..that connector i hv connected to pc

0 件の賞賛
返信

3,489件の閲覧回数
Nuevo
Contributor I

Hi

Dump Flash also succeeded......... but still our board is not bring up...... in nor flash some junk data is their............

0 件の賞賛
返信

3,490件の閲覧回数
addiyi
NXP Employee
NXP Employee

Can you please attache memory dump file?

Also, as NOR is memory mapped you can use Memory View to check if programming flash is done ok. If u-boot is correct written is flash, please check the connection of serial cable between PC and board.

Adrian

0 件の賞賛
返信

3,490件の閲覧回数
Nuevo
Contributor I

Hi

Connection is proper ...... some junk data is dumpping into flash ............ here am unable to attach the file......how to use memory view to check the programming flash

0 件の賞賛
返信

3,490件の閲覧回数
addiyi
NXP Employee
NXP Employee

In Debug, open Memory View (Window -> Show View -> Memory), then go to Memory tab and Add Memory Monitor and Enter address to monitor (in your case 0xFFF80000).

Adrian

0 件の賞賛
返信

3,490件の閲覧回数
Nuevo
Contributor I

4.1.1 NOR flash memory map address

Start Address         End Address       Description                                                  Size

0xef00_0000            0xef03_ffff        Vitesse 7385 Switch Firmware                         256K

0xef04_0000            0xef07_ffff        dtb image                                                       256K

0xef08_0000            0xef3f_ffff         uImage                                                           3.5M

0xef40_0000            0xefef_ffff       JFFS2 image                                                    11M

0xeff0_0000             0xefff_ffff         u-boot(at eff80000) and it's env (at eff60000)       1M

0 件の賞賛
返信

3,490件の閲覧回数
Nuevo
Contributor I

Hi

In Memory Tab Add Memory Monitor is disabled unable to add the address

0 件の賞賛
返信

3,490件の閲覧回数
addiyi
NXP Employee
NXP Employee

Board should be in Debug mode, to be able to Add Memory Monitor.

0 件の賞賛
返信

3,490件の閲覧回数
Nuevo
Contributor I

MEMORY.png

Hi

i have attached the memory view...... please can u go through....

0 件の賞賛
返信

3,490件の閲覧回数
Nuevo
Contributor I

fl::target -lc "FLASH-core00_RAM_P1020_Download"

fl::target -b 0x2000 0x30000

fl::target -v on -l off

cmdwin::fl::device -d "S29GL128P" -o "8Mx16x1" -a 0xff000000 0xffffffff

cmdwin::fl::image -f "C:\\Freescale\\BSP image\\P1020RDB_Images\\P1020RDB\\Pre_Build_images\\vsc2bin" -t "Binary/Raw Format" -re off -oe on -o 0xff7fe000

cmdwin::fl::erase image

Beginning Operation ...   

-------------------------

Performing target initialization ...   

Downloading Flash Device Driver ...  

Reading flash ID ...

Erasing Sector 0xFF7E0000 to 0xFF7FFFFF  

Erasing ...

Erase Command Succeeded   

cmdwin::fl::write verify

Beginning Operation ...   

-------------------------

Programming file C:\Freescale\BSP image\P1020RDB_Images\P1020RDB\Pre_Build_images\vsc2bin  

Downloading Flash Device Driver ...  

Reading flash ID ...

Downloading 0x00001FF8 bytes to be programmed at 0xFF7FE000  

Executing program with verify ....  

Program with Verify Command Succeeded   

cmdwin::fl::image -f "C:\\Freescale\\BSP image\\P1020RDB_Images\\P1020RDB\\Pre_Build_images\\u-boot_nor.bin" -t "Binary/Raw Format" -re off -oe on -o 0xfff80000

cmdwin::fl::erase image

Beginning Operation ...   

-------------------------

Downloading Flash Device Driver ...  

Reading flash ID ...

Erasing Sector 0xFFF80000 to 0xFFF9FFFF  

Erasing Sector 0xFFFA0000 to 0xFFFBFFFF  

Erasing Sector 0xFFFC0000 to 0xFFFDFFFF  

Erasing Sector 0xFFFE0000 to 0xFFFFFFFF  

Erasing .....

Erase Command Succeeded   

cmdwin::fl::write verify

Beginning Operation ...   

-------------------------

Programming file C:\Freescale\BSP image\P1020RDB_Images\P1020RDB\Pre_Build_images\u-boot_nor.bin  

Downloading Flash Device Driver ...  

Reading flash ID ...

Downloading 0x00010000 bytes to be programmed at 0xFFF80000  

Downloading 0x00010000 bytes to be programmed at 0xFFF90000  

Executing program with verify ....  

Program with Verify Command Succeeded   

Downloading 0x00010000 bytes to be programmed at 0xFFFA0000  

Downloading 0x00010000 bytes to be programmed at 0xFFFB0000  

Executing program with verify ....  

Program with Verify Command Succeeded   

Downloading 0x00010000 bytes to be programmed at 0xFFFC0000  

Downloading 0x00010000 bytes to be programmed at 0xFFFD0000  

Executing program with verify ....  

Program with Verify Command Succeeded   

Downloading 0x00010000 bytes to be programmed at 0xFFFE0000  

Downloading 0x00010000 bytes to be programmed at 0xFFFF0000  

Executing program with verify ....  

Program with Verify Command Succeeded   

cmdwin::fl::dump -range 0xff000000 0xffffffff -t "Binary/Raw Format" -o "C:\\Freescale\\BSP image\\P1020RDB_Images\\P1020RDB\\Pre_Build_images\\u-boot_nor.bin"

Beginning Operation ...   

-------------------------

Downloading Flash Diagnostics Driver ...  

Reading flash ID ...

Dumping flash region: 0xFF000000 - 0xFFFFFFFF to C:\Freescale\BSP image\P1020RDB_Images\P1020RDB\Pre_Build_images\u-boot_nor.bin  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Running Dump Flash ...  

Dump Flash Succeeded

0 件の賞賛
返信

3,490件の閲覧回数
Nuevo
Contributor I

Hi

can u please tell me the step to follow the nor flash programming

0 件の賞賛
返信