Opcode of  sub.l

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Opcode of  sub.l

5,715 次查看
JoeChou
Contributor I

I am running into a weird problem. The result of a ubtraction is supposed to be positive, but I got

negative value. It looks to me that the Compiler might havegenerated wrong assembly code, or the

assembler might have generated wrong Opcode.

 

Need ColdFire experts to teach us how the following Opcode works.


0x91AEFFE0    ub.l    d0,-32(a6)



Opcode is:    0x91AEFFE0


Assembly issub.l   d0,-32(a6)


 

Is it doing

 

-32(a6) =  -32(a6) - d0


OR,


-32(a6) = d0 - ( -32(a6) )


OR, it is doing something else ?



Regards,

Joe
标签 (1)
标记 (1)
0 项奖励
回复
11 回复数

3,237 次查看
Harjit
Contributor II

Does this happen for all subtractions of the form:

a = b-a;

 

or only for

*(a) = b - *(a);

 

or only for the condition where b is a constant?

 

or?

Thanks.

0 项奖励
回复

3,237 次查看
jbezem
Contributor III

Look at CFPRM.pdf in {install}\Freescale_Documentation, page 151 (I'm using CW7.1.1).

The Opmode is 110, therefore

  <ea>x - Dy --> <ea>x

in your case:

  (-32<a6>) -D0 --> (-32<a6>)

 

HTH,

 

Johan

0 项奖励
回复

3,237 次查看
JoeChou
Contributor I

Here is the C code, and the assembly code generated by CodeWarrior compiler.

 

T3_new = ATP_Timer_Get_10ms() - T3_new;


0x00009C98   0x4EB900009F88     jsr      0x00009f88

0x00009C9E   0x91AEFFE0         sub.l    d0,-32(a6)

 

0 项奖励
回复

3,237 次查看
CrasyCat
Specialist III

Hello

 

If you think the compiler is generating invalid code, I would recommend you to submit a service request for that.

Click here to submit a service request.

Make sure to attach a reproducible project and installed product information to the service request.
To generate the required information:
- Start CodeWarrior
- Open the project
- Select "Help" -> "Pack and Go" and follow instructions on the screen.

Attach the generated .zip file to the SR.

CrasyCat

0 项奖励
回复

3,237 次查看
jbezem
Contributor III

Did anyone follow-up on this one and generate a service request? I seem to have come across a similar problem...

 

Any feedback is welcome.

 

Thx,

 

Johan

0 项奖励
回复

3,237 次查看
JoeChou
Contributor I

Yes, the technical support guys have confirmed that the C Compiler generated wrong code.

 

This is indeed a compiler bug.

 

Regards,

Joe

0 项奖励
回复

3,237 次查看
jbezem
Contributor III

OK, thanks. Any reference number or even a version where the issue is or will be fixed?

 

Regards,

 

Johan

0 项奖励
回复

3,237 次查看
jbezem
Contributor III

OK, this turns out to be more serious: The command-line compiler seems to produce this error even when optimization is turned off.

A small example program to reproduce this:

void testfn(unsigned long * fn_param)
{
  *(fn_param) = 247 - *(fn_param);
}

/* Command line:
mwccmcf.exe -c -g -opt none,dump -dis -o testpeep.dis testpeep.c
*/

This produces the following code:

 

;    3:   *(fn_param) = 247 - *(fn_param);
;
0x00000008  0x203C000000F7           move.l   #247,d0               ; '....'
0x0000000E  0x9190                   sub.l    d0,(a0)

I tried some other options, but the result is always the same.

I'll filea bug report for this, since I know of no workaround, and this therefore means that our command-line based make-system will produce invalid code.

 

If someone finds a workaround for this problem (using the command-line compiler) I'd be very interested!

 

Regards,

 

Johan

 

 

0 项奖励
回复

3,237 次查看
jbezem
Contributor III

A summary:

The command-line compiler uses peephole optimization by default, even if '-opt none' is issued.

This optimization method contains the error as described above.

The documentation is in error, in that '-opt [no]peep[hole]' is not supported and results in an error. Instead, a separate option '-[no]peep[hole]' is available on the command line, as is correctly described in the command-line help using "mwccmcf -help". This option has to be indicated separately, and is not connected to the '-opt' option variants.

 

So, to avoid the error above when using the command-line compiler, specify '-nopeephole'.

 

The error is known at Freescale and registered under ID MTWX31403, to be resolved in the next few months: "... should be released before Q3".

 

HTH,

 

Johan

0 项奖励
回复

3,237 次查看
JoeChou
Contributor I

Dear Johan,

 

Your help is deeply appreciated. Unfortunately,  your answer also confirm our suspicion

on the compiler/assembler problem. Due to unknown reason, the CodeWarrior for ColdFire

Development Tool generated this wrong opcode. 

 

We have learned that there are at least two methods to avoid this compiler problem.

The first method is to change Global Optimizations to level 4.

The second method is to uncheck Peephole option under ColdFire Processor.

 

Thanks again.

 

Regards,

Joe

0 项奖励
回复

3,237 次查看
jbezem
Contributor III

Can you elaborate or provide a link as to the incorrect code generated? Source and disassembly, if possible?

TIA,

 

Johan

0 项奖励
回复