No probe connection for Codewarrior Tap

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

No probe connection for Codewarrior Tap

2,874件の閲覧回数
cengizhanyapici
Contributor I

In my bareboard application I want to use Codewarrior development studio although when I create a new project and debug it I take an error which is "CCSProtocolPlugin:Could not connect to the probe(or other debug link)

[CCS last error:CC not present ]"

Then,I run the necessary COM port from TerraTerm application and I see "No probe connection" message on the screen.Is the problem related to this "No probe connection" message which is given as attached? or Is there some problem about CodeWarrior's connections? Thanks for your answers.

 

Best Ragards

ラベル(1)
0 件の賞賛
返信
1 返信

2,570件の閲覧回数
addiyi
NXP Employee
NXP Employee

What connection you are setting in CW for cwtap?

Adrian

0 件の賞賛
返信