New to Coldfire and Codewarrior

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

New to Coldfire and Codewarrior

跳至解决方案
2,811 次查看
hpi_2
Contributor I

Hi,

 

I'm new to Coldfire and recently accuired a M52259DEMO dev board. 

 

Coming from a MICROCHIP 8-bit background, where can I start? I did following the GETTING STARTED pdf that came with the  M52259DEMO dev board. Its nice to see an application, but where can I start learning the environment? How do I setup register?

 

For example, the Coldfire comes with the MQX RTOS, how does one use the micro without the MQX...like only flashing a led?

 

If you can suggest any tutorials, books etc ?

 

Thanks,

Eben 

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,701 次查看
Nouchi
Senior Contributor II

Hello Eben,

 

First, welcome to the 32 bits world!!!

 

 You can fin all you need on Freescale web site, but I suggest you some link like :

- The MCF5225x Reference Manual

- The Data Sheet

For The MQX RTOS, you can find documentation in "C:\Program Files\Freescale\Freescale MQX 3.1\doc" folder.

Useful informations about CodeWarrior are here : "C:\Program Files\Freescale\CodeWarrior for ColdFire V7.1\Help\PDF"

I recommend MSL_C_Reference.pdf, Targeting_ColdFire.pdf, and the excellent ColdFire_Build_Tools_Reference.pdf (especially chapter 19 about runtime libraries)

 

 

Emmanuel

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,702 次查看
Nouchi
Senior Contributor II

Hello Eben,

 

First, welcome to the 32 bits world!!!

 

 You can fin all you need on Freescale web site, but I suggest you some link like :

- The MCF5225x Reference Manual

- The Data Sheet

For The MQX RTOS, you can find documentation in "C:\Program Files\Freescale\Freescale MQX 3.1\doc" folder.

Useful informations about CodeWarrior are here : "C:\Program Files\Freescale\CodeWarrior for ColdFire V7.1\Help\PDF"

I recommend MSL_C_Reference.pdf, Targeting_ColdFire.pdf, and the excellent ColdFire_Build_Tools_Reference.pdf (especially chapter 19 about runtime libraries)

 

 

Emmanuel

 

0 项奖励
回复
1,701 次查看
hpi_2
Contributor I

Hi Emmanuel,

 

Thanks for the suggestions. I will certainly study the mentioned documents.

 

Thanks! :smileywink:

0 项奖励
回复