NAND, NOR Memory programs for (QorlQ) P2020

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NAND, NOR Memory programs for (QorlQ) P2020

1,184 Views
nareshpuli
Contributor III

Hi,

 

how we write NAND, NOR Memory programs for P2020(QorlQ) Processor

how we start the program and how we difine headers ?

Labels (1)
0 Kudos
Reply
1 Reply

948 Views
Pavel
NXP Employee
NXP Employee

Evaluation version of CodeWarrior can be used during 30 days. There are no other limitations for using evaluation version.

Use evaluation version CodeWarrior for Flash programming on your board.

NZP offers CodeWarrior Eclipse edition v 10.5.1:

http://www.nxp.com/products/software-and-tools/software-development-tools/codewarrior-development-to...

 

NZP also offers CodeWarrior Classic edition v 8.8:

http://www.nxp.com/products/software-and-tools/software-development-tools/codewarrior-development-to...

 

These compilers support the P2020.

 

Documentation for CodeWarrior Eclipse edition contains information for Flash programmer in CodeWarrior folder. See the Chapter 11 in the following file:

Find Targeting_PA_Processors.pdf

 

Documentation for CodeWarrior 8.8 contains information for Flash programmer in CodeWarrior folder.

See the Chapter 5 in the following file:

Pro & Linux App Edition Targeting Manual.pdf


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply