Most recent CW release for ARMv7?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Most recent CW release for ARMv7?

1,954 Views
mindchasers
Contributor III

Hello,

What is the most recent CW release that will support ARMv7 (LS1021A)? 

It looks like CW4NET_v2018.01 doesn't support it even though it is listed under CW for QorIQ LS ARMv7 ISA on nxp.com.

Also, will CW support LS1021A into the future, or is it being dropped?

Thank you,

Bob

0 Kudos
Reply
2 Replies

1,783 Views
yipingwang
NXP TechSupport
NXP TechSupport

The latest CodeWarrior for ARMv7 provided in CW4NET_v2017.03 is 10.0.9.

You could update CodeWarrior for ARMv7 with the online updater.

In CodeWarrior IDE, please open Help->Install New Software, click "Available Software Sites" to check "CW ARMv7 Updates", please click drop down icon at "Work with:", and select "CW ARMv7 Updates - http://cache.nxp.com/lgfiles/updates/Eclipse/ARMv7_10_0_9/Windows", then check "CodeWarrior Updates" to follow the new project wizards to update CodeWarrior step by step.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,783 Views
addiyi
NXP Employee
NXP Employee

CodeWarrior for ARMv7 is available in CW4NET2017.03 installer. Also, the updates are provided via update sites. LS1021A is supported.

Adrian

0 Kudos
Reply