Most recent CW release for ARMv7?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Most recent CW release for ARMv7?

1,967件の閲覧回数
mindchasers
Contributor III

Hello,

What is the most recent CW release that will support ARMv7 (LS1021A)? 

It looks like CW4NET_v2018.01 doesn't support it even though it is listed under CW for QorIQ LS ARMv7 ISA on nxp.com.

Also, will CW support LS1021A into the future, or is it being dropped?

Thank you,

Bob

0 件の賞賛
返信
2 返答(返信)

1,796件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

The latest CodeWarrior for ARMv7 provided in CW4NET_v2017.03 is 10.0.9.

You could update CodeWarrior for ARMv7 with the online updater.

In CodeWarrior IDE, please open Help->Install New Software, click "Available Software Sites" to check "CW ARMv7 Updates", please click drop down icon at "Work with:", and select "CW ARMv7 Updates - http://cache.nxp.com/lgfiles/updates/Eclipse/ARMv7_10_0_9/Windows", then check "CodeWarrior Updates" to follow the new project wizards to update CodeWarrior step by step.


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,796件の閲覧回数
addiyi
NXP Employee
NXP Employee

CodeWarrior for ARMv7 is available in CW4NET2017.03 installer. Also, the updates are provided via update sites. LS1021A is supported.

Adrian

0 件の賞賛
返信