Modify "Include" Folder

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Modify "Include" Folder

跳至解决方案
1,470 次查看
Kafre
Contributor III

Hello all,

 

I use Codewarrior 10 for MCU with MQX 3.6.2

 

I'm importing a MQX "BSP build" project and modifying it to use it with a different MCU. After changing the Path variables, the linked  resources and the CF compiler and assembler inputs to desired ones, I found that the "Includes" folder under the built project (aka bsp_<put_your_mcu_here>) was unchanged. This means that my Includes were pointing to the older Includes. (eg c:\program files\freecake\mqx\sources\io\etc instead of d:\my super sources\my super includes\io\etc)

 

The thing is, that I think that when the linking and compiling is made, the inclusion points the new files, but the reference in the Include folder is still the old one and if I try to open the files included there, they are just empty files. My attempts to change the folder or even eliminate it, have been unsuccessful. Is there a way to change this?

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,015 次查看
Kafre
Contributor III

Ok, I found it. I just have to create a new "Build Variable" to avoid the includes from pointing the c drive archives.

 

Note to self: Add Build Variables to all projects, new paths are not enough.

 

Solved!

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,016 次查看
Kafre
Contributor III

Ok, I found it. I just have to create a new "Build Variable" to avoid the includes from pointing the c drive archives.

 

Note to self: Add Build Variables to all projects, new paths are not enough.

 

Solved!

0 项奖励
回复