MPC860 configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC860 configuration

3,454件の閲覧回数
jjbloomi
Contributor I
I am looking for a sample Codewarrior target initialization file for the MPC860. 
I am using dev board STK8xx from TQ Components with an MPC860 mini-module.
Codewarrior version 5.7.0 with Ethernet Tap.  The BDM directory referred to in the documentation is
not included in this version of CW and I assume that the 860 must have been obsoleted.
 
 
ラベル(1)
タグ(1)
0 件の賞賛
返信
3 返答(返信)

1,887件の閲覧回数
Voxan
Contributor III
Hi Jjbloomi,

the latest CodeWarrior version is v8.7, released last week.

I just checked and the particular board/core you are asking for is not supported.
If you want to go forward, you may want to edit one of the 8xx provided initialization file and adapt it to your board.

Hope this helps...

Best Regards
0 件の賞賛
返信

1,887件の閲覧回数
Muneer
Contributor II
Hi


I'm also using CW8.7 and MPC860 PC I
Can u give some example for 8xx cfg files
Is it possible to Initialize Ports(8xx) in cfg files?


Message Edited by Muneer on 2008-02-14 06:52 AM

1,887件の閲覧回数
CrasyCat
Specialist III
Hello
 
You can find example of .cfg files for MPC8xx in {Install}\PowerPC_EABI_Support\Initialization_Files\PQ1 (where {Install} refers to your installation directory).
 
You can find more information on commands you can use in the .cfg file in "{Install}\Help\PDF\Pro & Linux App Edition Targeting Manual.pdf" in chapter "Target Initialization File".
 
As stated there "A target initialization file is a file that contains commands that initialize registers, memory
locations, etc. on a target board."
 
CrasyCat
0 件の賞賛
返信