MPC55xx: Problem to generate .sym

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC55xx: Problem to generate .sym

3,083 Views
mudy
Contributor I
Hello. I'm using Freescale Codewarrior for MPC55XX ver. 2 and my operating system is Windows XP.

After the command "Make" I would want also a file .sym. But this file isn't generated!

I read the CodeWarrior Help to create a symbolics file (.sym) and the step number 4 is:

4)For Macintosh PowerPC, select PPC Linker in the Target Settings Panels list (Linker group), then enable Generate SYM File.

...but:
1) I have EPPC Linker and not PPC linker,
2) In EPPC Linker there isn't the command (or option) "Generate SYM File".

What can I do?

Thanks

Message Edited by CrasyCat on 2007-04-13 01:49 PM

Labels (1)
0 Kudos
Reply
4 Replies

1,143 Views
CrasyCat
Specialist III
Hello
 
What is the purpose of the .sym file you are looking  for?
CodeWarrior for MPC55xx generates an ELF DWARF executable file.
 
This file is compliant to the ELF DWARF standard file format. Why do you need a .sym file?
And which format is that file expected to have?
 
CrasyCat
0 Kudos
Reply

1,143 Views
mudy
Contributor I
Hello.

I would want a file .sym or .elf to debug the project.

But, after the command "MAKE", a file .elf isn't generated.

Which is the procedure to obtain the file .elf?

thanks
0 Kudos
Reply

1,143 Views
CrasyCat
Specialist III
Hello
 
You can find the name of the generated executable file in the "EPPC Target" panel.
This file is generated in the output directory specified in the Output Directory specified in the "Target Settings" panel. 
 
The file specified there is an ELF DWARF executable file and is what you are looking for.
 
If you have created your project using a stationery, the elf file is called Simple.out and is located
in your project bin directory.
 
You can rename the file in the EPPC Target" panel if you wish.
I hope this helps.
 
CrasyCat
0 Kudos
Reply

1,143 Views
mudy
Contributor I
Ok!

Thanks

mudy
0 Kudos
Reply