MPC5553: FLASH ERASE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5553: FLASH ERASE

8,368件の閲覧回数
mudy
Contributor I
Hello!

I'm using Mpc5553 and I would want to erase the flash. In the reference manual there's the correct sequence of events for this operation. The step n°3 is:

3) Write to any address in flash. This is referrred to as an erase interlock write.

My code for an erase interlock write is like that:

*address=value;


...but this line of code reset the system!

The block of flash to be erased doesn't contain code and it's correctly selected and it isn't locked.

Can you help me?

Thanks

Mudy

Message Edited by Alban on 2006-11-02 03:36 PM

ラベル(1)
タグ(1)
0 件の賞賛
返信
10 返答(返信)

4,991件の閲覧回数
nerdstuff
Contributor II

I have the same problem.  When performing the erase interlock write, I get a bus error. Any insight on why that would be? I am on an MPC5602P. I have verified through the code flash registers that the block is both unlocked and selected for erase. When I write to 0x0000000, I get a bus error.  The freescale driver seems to have the same issue.

0 件の賞賛
返信

4,991件の閲覧回数
J2MEJediMaster
Specialist I
Does the Coldfire architecture still require certain accesses to be on word boundaries? Is this address you're writing to an odd address? Maybe you're triggering a bus error. Sorry, that's just my scientific wild guess as to how a single write would circumvent all of the other safeguards and bring the processor down...

---Tom
0 件の賞賛
返信

4,991件の閲覧回数
mudy
Contributor I
The problem isn't solved...It's the same!

regards

mudy
0 件の賞賛
返信

4,991件の閲覧回数
J2MEJediMaster
Specialist I
Have you tried looking at App note AN3283, which discusses erasing flash on MPC5500 family?

It's located here.

---Tom
0 件の賞賛
返信

4,991件の閲覧回数
mudy
Contributor I
Yeah i read tihs application notes, but I don't want erase (or program) the flash trogh the Nexus\jtag port. I would want to write a program that use the flash for data. I'm trying to erase a block of high address space.

I started trying to erase the flash. In the reference manual of mpc5553 I read:

The erase sequence consists of the following sequence of events:
1. Change the value in the FLASH_MCR[ERS] bit from 0 to a 1.

2. Select the block, or blocks to be erased by writing ones to the appropriate registers in
FLASH_LMSR or FLASH_HSR.
NOTE:
Lock and Select are independent. If a block is selected and locked, no erase
will occur.

3. Write to any address in Flash. This is referred to as an erase interlock write.

4. Write a logic 1 to the FLASH_MCR[EHV] bit to start an internal erase sequence or skip to step 9
to terminate.

5. Wait until the FLASH_MCR[DONE] bit goes high.

6. Confirm FLASH_MCR[PEG] = 1.

7. Write a logic 0 to the FLASH_MCR[EHV] bit.

8. If more blocks are to be erased, return to step 2.

9. Write a logic 0 to the FLASH_MCR[ERS] bit to terminate the erase.


My code is attached.
...but at the step 3 (interlock write)at the first access to the flash the system shut down. I try at the step 2 also this instruction:

FLASH.HSR.B.HBSEL=134217728; // 134217728= 2 ^27

but the problem is the same.

I'm sorry for my terrible english...

thanks

mudy
0 件の賞賛
返信

4,992件の閲覧回数
tomtomtom
Contributor I

Does anybody solved the problem? and succed to write into flash?

 

Thanks

0 件の賞賛
返信

4,992件の閲覧回数
abdellatif_elou
Contributor I

I use MPC555, and I've deselect  CMF B FROM FLASH MEMORY  by error (now i have only ???????? from 0x40000 to 0x6FFFF) . so I want to select this block to errase it. i found these steps but i don't know if that resolved the problem.

 

To set one or both of the bits in CENSOR[0:1],
1. Using section 19.7.6 A Technique to Determine SCLKR, CLKPE, and
CLKPM, write the pulse width timing control fields for an erase pulse, CSC = 1,
PE = 0 and SES = 1 in the CMFCTL register.
2. Write a one to the CENSOR bit(s) to be set.
3. Write EHV = 1 in the CMFCTL register. This will apply the programming voltages
to NVM bit 0 and the erase voltages to NVM bit 1 simultaneously.
4. Read the CMFCTL register until HVS = 0.
5. Write EHV = 0 in the CMFCTL register.
6. Read the CMFMCR CENSOR bit(s) that are being set. If any bit selected for set
is a 0 go to step 3.
7. Write SES = 0 and CSC = 0.

 

can someone help me to set CENSOR[0:1] to no censorship (01 or 10).

thanks for help

0 件の賞賛
返信

4,992件の閲覧回数
MCF52233
Contributor III

Hi ,

 

Just doing guesswork.

 

try to disable interrupt before erasing flash.

Let us know if it works or not.

 

Regards,

0 件の賞賛
返信

4,992件の閲覧回数
abdellatif_elou
Contributor I

hi,

I can't do the example presented in 19.7.6 A Technique to Determine SCLKR, CLKPE, and

CLKPM, to clear or set censorship. MPC555 works at 10MHZ, and when set clock frequency more than 20 Mhz, the target goes to reset. so what are the values to be take for SCLKR, CLKPE, CLKPM ans PAWS to clear first Censor, then set it to no censor ship  switch this procedure:

To clear CENSOR[0:1],
1. Write PROTECT[0:7] = 0x00 to enable the entire array for erasure.
2. Using section 19.7.6 A Technique to Determine SCLKR, CLKPE, and
CLKPM, write the pulse width timing control fields for an erase pulse,
BLOCK[0:7] = 0xFF, CSC = 1, PE = 1 and SES = 1 in the CMFCTL register.
3. Perform an erase interlock write.
4. Write EHV = 1 in the CMFCTL register. This will apply the erase voltages to the
entire CMF array and NVM bit 0 and the programming voltages to NVM bit 1
simultaneously.
5. Read the CMFCTL register until HVS = 0.
6. Write EHV = 0 in the CMFCTL register.
7. Read the entire CMF array and the shadow information words. If any bit equals
zero, go to step 4.
8. Read CENSOR[0:1]. If CENSOR[0:1] ≠ 0 go to step 4.
9. Write SES = 0 and CSC = 0.

 

trying to disable interrupt before erasing flash don't resolve the problem. have you more details please ?

thanks for help

0 件の賞賛
返信

4,992件の閲覧回数
jonr
Contributor III
0 件の賞賛
返信