MPC5121 unable to function properly, and the program step at 0x00000204.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5121 unable to function properly, and the program step at 0x00000204.

1,710 Views
hensonJhon
Contributor I

The DDR model used is EM68C08CWAG-25H, and the register values can be read correctly in codewarrior. when debugging the program, the program will be stuck at 0x00000800 and can NOT run forward.

About the .cfg I used the codewarrior 9.2 file like(DIR\Freescale\CodeWarrior for MobileGT V9.2\PowerPC_EABI_Support\Initialization_Files\52xx\5121ADS_init.cfg).

but it also does not work.

so,I wanna try to use the sram moudle to program the code, and the program step at 0x00000204.

in the process of the configure, i change the code link command and 5121ADS_init.cfg as the shown of the pictures.but it also doesn't work.

so whats the meaning of this condition? how can i do in the next work?

thank u.

0 Kudos
Reply
0 Replies