M52259Demo MQX_3_7 - Flash Programmer: The Debugger can not write to memory

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

M52259Demo MQX_3_7 - Flash Programmer: The Debugger can not write to memory

872 次查看
PavelPin
Contributor I

Configuration:

Win 7 Prof

CodeWarior 7.2 Eval.  + Patch 722

Project MQX + MFS (I also tested "only MQX")

Flash Programer :

52259 / Coldfire v2-v4 JM60 OSBDM

Target inic ...ColdFire_Support\Initialization_Files\M52259DEMO.cfg

Erase Flash  :  Erase Command Succeeded  

Blank Check Completed Successfully 

--------

Program/Verify

...MQX_3_7Test_MFS\output\intflash_d.elf.S19

Program

Downloading 0x00010000 bytes to be programmed at 0x00000420 

The Debugger can not write to memory

How to ?

 

Thank Pavel

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

684 次查看
PavelPin
Contributor I

Hi

For example, FreeRTOS ok writed to internal Flash.

0 项奖励
回复