M52233Demo Board with Codewarrior v10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

M52233Demo Board with Codewarrior v10

2,097件の閲覧回数
Masmiseim
Senior Contributor I

Hello,

 

I Try to use the M52233Demo Board with Codewarrior v10, using the BDM on the Evalboard.

Windows recognize the Board as “Jungo USB Multilink 2.0” in the Device Manager.

I ‘m not able to get a connection to the BDM in Codewarrior.

I’ve tried OSBDM ==> Error: “Coldfire GDI Protocol Adapter: Can’t connect. The Debugger can not load the OSBDM DLL!

And PnE BDM ==> Error: “Coldfire GDI Protocal Adapter: Can’t connect. The Debugger can not connect to the PE BDC interface or targeted hardware board.

 

Any suggestion?

 

Greetings

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,416件の閲覧回数
Masmiseim
Senior Contributor I

Hello again.

I've tryed this Errata:

http://cache.freescale.com/files/community_files/OSBDM08/OSBDM_ERRATA.pdf?fsrch=1&sr=1

 

While using the jm60_fwinfo.exe, I get the Error: "Can't find a OSBDM-JM60 USB device.".

Either I’ve the wrong driver. But as mentioned above it is recognized as “Jungo USB Multilink 2.0” in the Device Manager.

Or, on this Board is not an OSBDM, but something else …

 

0 件の賞賛
返信