M52233Demo Board with Codewarrior v10

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

M52233Demo Board with Codewarrior v10

2,099 次查看
Masmiseim
Senior Contributor I

Hello,

 

I Try to use the M52233Demo Board with Codewarrior v10, using the BDM on the Evalboard.

Windows recognize the Board as “Jungo USB Multilink 2.0” in the Device Manager.

I ‘m not able to get a connection to the BDM in Codewarrior.

I’ve tried OSBDM ==> Error: “Coldfire GDI Protocol Adapter: Can’t connect. The Debugger can not load the OSBDM DLL!

And PnE BDM ==> Error: “Coldfire GDI Protocal Adapter: Can’t connect. The Debugger can not connect to the PE BDC interface or targeted hardware board.

 

Any suggestion?

 

Greetings

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,418 次查看
Masmiseim
Senior Contributor I

Hello again.

I've tryed this Errata:

http://cache.freescale.com/files/community_files/OSBDM08/OSBDM_ERRATA.pdf?fsrch=1&sr=1

 

While using the jm60_fwinfo.exe, I get the Error: "Can't find a OSBDM-JM60 USB device.".

Either I’ve the wrong driver. But as mentioned above it is recognized as “Jungo USB Multilink 2.0” in the Device Manager.

Or, on this Board is not an OSBDM, but something else …

 

0 项奖励
回复