M52233DEMO board problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

M52233DEMO board problem

1,685件の閲覧回数
yucheng
Contributor I

I build the evaluation project with code warrior for this board, but got problem for debug, program not stop even set breakpoint at start of main(). Do I need to do any environment settings before debug?

btw, for this board, what's the settings for flash programmer?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

977件の閲覧回数
MCF52233
Contributor III

hi yucheng,

which eval project u tried??

what is the size of ur code??

if it is greater than 32K then u hv to target for flash.i.e 1st program the KIT then start debug.

0 件の賞賛
返信