Linux cross tools are missing in CodeWarrior ARMv7 2019.01

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Linux cross tools are missing in CodeWarrior ARMv7 2019.01

ソリューションへジャンプ
3,523件の閲覧回数
miloserdin
Contributor I

Hello!

I've installed CodeWarrior ARMv7 2019.01 (from CW_ARMv7_v2019.01_b190131_Win_Offline.exe file) and tried to create Linux application project. But it's failed due to missing Linux cross tools installed. I've checked the updates but nothing was found.

Where can I get Linux cross tools to use with CodeWarrior ARMv7 2019.01?

Best regards,

Oleg

0 件の賞賛
返信
1 解決策
3,508件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

GCC Linaro Linux Toolchain is not provided for CodeWarrior ARMv7, you also cannot find it in CodeWarrior online updater.

You could use Linux edition GCC Linux Toolchain provided in Linux SDK to build your Linux project.

Please download "QorIQ Linux SDK v2.0 AARCH64 IMAGE" ISO from https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/linux-sdk...

Then install the script in fsl-toolchain folder to install GCC Linux toolchain.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,509件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

GCC Linaro Linux Toolchain is not provided for CodeWarrior ARMv7, you also cannot find it in CodeWarrior online updater.

You could use Linux edition GCC Linux Toolchain provided in Linux SDK to build your Linux project.

Please download "QorIQ Linux SDK v2.0 AARCH64 IMAGE" ISO from https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/linux-sdk...

Then install the script in fsl-toolchain folder to install GCC Linux toolchain.

0 件の賞賛
返信
3,505件の閲覧回数
miloserdin
Contributor I

Hi, @yipingwang !

OK, I see.

If I'm going to use only ARMv7 CPU (i.e. LS1021A) should I download "QorIQ Linux SDK v2.0 CORTEXA7 IMAGE" instead of "QorIQ Linux SDK v2.0 AARCH64 IMAGE"?

Best regards,

Oleg

0 件の賞賛
返信
3,493件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Yes, please download "QorIQ Linux SDK v2.0 CORTEXA7 IMAGE".

0 件の賞賛
返信