License problem with evaluation version of 7.2

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

License problem with evaluation version of 7.2

1,531 次查看
ARQ
Contributor I

I installed CodeWarrior for Coldfire 7.2 Special Edition and MQX 3.5.1 to try the demo projects for the MCF52259 tower kit.  This was installed clean on a Windows XP 32-bit system, and no other CodeWarrior versions were installed on this system previously.

 

The project (...MQX 3.5\demo\hvac\cwcf72\hvac_twrmcf52259.mcp) compiles fine but when I go to program the Flash, I get the following error:  "Nothing downloaded, limited to 131072 bytes of code." 

 

I understand the special version is limited to 128kb code size, but I thought this restriction is not there for the first 30 days.  I was doing this testing the same day I installed it.

 

Any suggestions?

 

Thanks

标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

842 次查看
vier_kuifjes
Senior Contributor I

That's your problem: the "evaluation version" is not the same as the "special edition" version. The special edition version is free but limited to 128K of object code. The evaluation version, which is a different download, is unlimited for 30 days, after which it reverts to the special edition version.

 

0 项奖励
回复

842 次查看
ARQuattr
Contributor IV

I see, thank you.  I misunderstood - I thought the special edition had no limitations for 30 days.

 

Thanks.

0 项奖励
回复