LS2088A Licence issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LS2088A Licence issue

2,045件の閲覧回数
vijaykumardesai
Contributor II

When i try to run hello world program on LS2088RDB board, i get the licence error as,

Processor: LS2088A
Probe: CodeWarrior TAP (127.0.0.1)
//
Additional error details:
[GTA: license checkout failed. Cannot find license file.
The license files (or license server system network addresses) attempted are
listed below. Use LM_LICENSE_FILE to use a different license file,
or contact your software provider for a license file.
Feature: ARMv8DBG
Filename: /opt/Freescale/CW4NET_v2017.03/CW_ARMv8/../Common/license.dat
License path: /opt/Freescale/CW4NET_v2017.03/CW_ARMv8/../Common/license.dat:
FlexNet Licensing error:-1,359. System Error: 2 "No such file or directory"
For further information, refer to the FlexNet Licensing documentation,
available at "www.flexerasoftware.com".]

I have 15 days trial period, why i am getting this error?

0 件の賞賛
返信
1 返信

1,814件の閲覧回数
addiyi
NXP Employee
NXP Employee

Check is license.dat is available in /Freescale/CW4NET_v2017.03/CW_ARMv8/../Common/. This is generated only first time when CW4NET is installed.

Adrian

0 件の賞賛
返信