Internal console support in CW 8.6 PPC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Internal console support in CW 8.6 PPC

2,569 Views
gabbayo
Contributor I
Hi,
 
I'm using CW 8.6 with an MPC8272 processor. I'm using the build-in console support, because I don't want to connect a physical cable to the board.
 
The internal console is working but it is working with extremely low speed. It takes a couple of seconds, instead less than one second,  to display just 7-8 lines of text.
 
Does anyone know how to increase the build-in speed ?
 
Thanks.
Labels (1)
0 Kudos
Reply
1 Reply

1,602 Views
Teo
NXP Employee
NXP Employee
You can increase speed on stdout printing by minimizing how often console flushing is done. For details on how this can be done see: http://forums.freescale.com/freescale/board/message?board.id=CWCOMM&message.id=1031
 
Regards,
Teo
0 Kudos
Reply