Can I automate flash programming for M52235EVB with CodeWarrior

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can I automate flash programming for M52235EVB with CodeWarrior

2,301 次查看
hdj100r
Contributor I
Hello,
 
I have a M52235EVB and am using CodeWarrior V6.3. Is there any way to automate the downloading program to flash after a successful make? The debugger seems to automate the downloading to RAM, but my program is too large for the RAM, and I need it in flash. It is becoming a real drag having to manually erase and then program the flash using the flash programmer tools.
 
Cheers
David 
标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,263 次查看
CrasyCat
Specialist III

Hello

It is not possible to automatically (or transparently) download code into flash when you hit the debug button.

I will forward that to our planning team as a possible improvement for a future release of the product.

CrasyCat

0 项奖励
回复