How to tell object code size in Codewarrior?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to tell object code size in Codewarrior?

ソリューションへジャンプ
2,548件の閲覧回数
vier_kuifjes
Senior Contributor I

I hope this is not a dumb question...

 

I was wondering how I can tell the exact object code size of a compiled and linked program in Codewarrior. Knowing that Codewarrior SE has a limited object code size, it is nice to know how much space is left for extra code.

 

I always thought the number a the bottom of the folders window in codewarrior was the number to watch for. But when compiling some of the MQX demo apps, this number sometimes far exceeds the total flash memory capacity of the CPU, so this can't be it. So... where is it?

 

And then I have the same question about the RAM memory usage. How to tell how much RAM is used by static allocation?

 

I hope someone can help!

Thanks in advance - Marc

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,603件の閲覧回数
vier_kuifjes
Senior Contributor I
Apparently what I need to know is in the XMAP file...

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,604件の閲覧回数
vier_kuifjes
Senior Contributor I
Apparently what I need to know is in the XMAP file...
0 件の賞賛
返信