How to open CCS console

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to open CCS console

ソリューションへジャンプ
4,581件の閲覧回数
nsutch
Contributor III

Hi,

I'm new to the CW software so forgive the basic question, but how do I open the CCS console to type commands?

We have a new design with a T1040 processor - this is the first time we have brought it up so no previous configuration existed. I've used the QCVS tool to generate the RCW and created a JTAG chain config file from the QCVS output. I've also configured a remote session to connect to the T1040 via the CodeWarrior Tap.

I'm getting an error (CCSProtocolPlugin : Failed to correctly configure JTAG chain). Looking at the CodeWarrior Tap console it shows ccs_error = 39. There appears to be similar situations on the community but most of them talk about entering commands such as '(bin) 1 % findcc cwtaps' into the CCS consolse. 

I can see the CCS as a background process in Windows Task Manager (I'm running Windows 8.1) but I can't see how to open it so that I can enter commands.

Running CodeWarrior Development Suite for Power Architecture v10.5.0

What am I doing wrong??

Thanks,

Nick

ラベル(1)
0 件の賞賛
返信
1 解決策
3,732件の閲覧回数
addiyi
NXP Employee
NXP Employee

ccs process can be found in the task bar. Double click on the ccs icon to open the console.

Adrian

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
3,733件の閲覧回数
addiyi
NXP Employee
NXP Employee

ccs process can be found in the task bar. Double click on the ccs icon to open the console.

Adrian

0 件の賞賛
返信