How many question about MCF52233DEMO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How many question about MCF52233DEMO

1,951 Views
o0Zz
Contributor I
Hi all world,
 
I'm a french student and I m interresting by the MCF52233DEMO but I have some questions :
 
Have you an exemple of application who use the network ? (Because i have download CodeWarrior for ColdFire V6.4) and I haven't find an exemple for use the network just for configuration (mac...).
 
The RTOS by defaut is multi task and have telnet?
 
Tanks you for you answer and sorry for my bad english !
Labels (1)
0 Kudos
Reply
1 Reply

1,052 Views
mjbcswitzerland
Specialist V
Hi

Please check out the uTasker project: www.uTasker.com

It contains a RTOS including TELNET and is free for educational use. It is delievered with a ready-to-run CW 6.3 project demonstrating dynamic web server, DHCP, DNS, FTP, SMTP, TELNET, UART, I2C, etc. It supports software uploads via HTTP post. It comes with the uTasker simulator which allows testing and debugging on a PC which simulates the M52233 DEMO or M52235 EVB.

Regards

Mark

www.uTasker.com

0 Kudos
Reply