How many question about MCF52233DEMO

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How many question about MCF52233DEMO

1,953件の閲覧回数
o0Zz
Contributor I
Hi all world,
 
I'm a french student and I m interresting by the MCF52233DEMO but I have some questions :
 
Have you an exemple of application who use the network ? (Because i have download CodeWarrior for ColdFire V6.4) and I haven't find an exemple for use the network just for configuration (mac...).
 
The RTOS by defaut is multi task and have telnet?
 
Tanks you for you answer and sorry for my bad english !
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,054件の閲覧回数
mjbcswitzerland
Specialist V
Hi

Please check out the uTasker project: www.uTasker.com

It contains a RTOS including TELNET and is free for educational use. It is delievered with a ready-to-run CW 6.3 project demonstrating dynamic web server, DHCP, DNS, FTP, SMTP, TELNET, UART, I2C, etc. It supports software uploads via HTTP post. It comes with the uTasker simulator which allows testing and debugging on a PC which simulates the M52233 DEMO or M52235 EVB.

Regards

Mark

www.uTasker.com

0 件の賞賛
返信