How can I use P2020DS initialization script, not using CW IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How can I use P2020DS initialization script, not using CW IDE

1,355件の閲覧回数
sajjadahmed
Contributor II

I'm writing an initialization script for P2020DS and I want to initialize it with standard configs, I'm using CodeWarrior Gigabit TAP probe but not the CodeWarrior IDE. It will be a good idea to use the script provided by the CW IDE if I can use it with other eclipse based IDE. Moreover is there any command line interface (CLI) with which I can use to read/write the P2020's registers?

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 返信

1,205件の閲覧回数
addiyi
NXP Employee
NXP Employee

Running the initialization script provided by CW IDE, but not in CW IDE is not possible, since the CW IDE is based on a proprietary debugger which converts the initialization command to be "understand" by ccs. You can convert the initialization script provided by CW IDE in a scripts using ccs commands and run the script from ccs.

Adrian

0 件の賞賛
返信