How Debug P1010

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How Debug P1010

1,624 Views
zerro_wei
Contributor I

I am debugging p1010 chip with CodeWarrior tap. How to configure CodeWarrior tap to adapt to p1010

0 Kudos
Reply
1 Reply

1,615 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please download and install CodeWarrior for PA 10.5.1 from the following link.

https://drive.google.com/file/d/18YIFeSnzZlcE1ZgSNUlTYM955gh9_B56/view?usp=sharing

Then refer to the section "3.2.1 Creating CodeWarrior Bareboard Application Project" and "3.4.1 Debugging Bareboard Application Projects" in C:\Freescale\CW_PA_v10.5.1\PA\Power Architecture Processors Getting Started Guide.pdf to create and debug a hello world bare board project.

In addition, during custom board bringing up stage, when you create a bareboard project following new project wizards, in "Debug Target Settings" panel, you could select "Download/Connect" SRAM Launch configuration to run the sample program in L2 Cache to SRAM to avoid configuring DDR controller according to your custom board.

0 Kudos
Reply