Help with NicheLite stack - CodeWarrior version 7.0 Build 7, MCF52235EVB

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Help with NicheLite stack - CodeWarrior version 7.0 Build 7, MCF52235EVB

2,585 次查看
sdesai
Contributor I
Has anyone gotten the NicheLite sample program to work with the free version of CodeWarrior that comes with the MCF52235EVB. Everytime I try to compile, I get the message that the license does not support the code size. Do I have to purchase the standard or professional edition of CodeWarrior just to get this example project to work? I appreciate any help. Thank you.
标签 (1)
标记 (1)
0 项奖励
回复
2 回复数

1,283 次查看
vier_kuifjes
Senior Contributor I
Strange... I have a couple of applications running under Coldfire Lite, based on AN3518. Compiles perfectly using Codewarrior for Coldfire, special edition. Resulting code size is about 121k I believe.

Your problem might be that the application you're compiling contains a web server, with the contents of the web pages (graphics and stuff) included in the source code as data arrays, which significantly increases the code size to an amount larger than the maximum allowed by the special edition compiler.

Otherwise, try to base your application on AN3470 or AN3518, but to compile these you might need Codewarrior for Coldfire version 6.4 as these don't compile correctly with version 7.0. (based on an older version of iNiche Coldfire Lite, with some bugs inside...).
It is possible to convert those application notes to use the most recent version of Coldfire lite though. I did, and now it works correctly compiled with CW7.0.
0 项奖励
回复

1,283 次查看
J2MEJediMaster
Specialist I
A code size error is definitely a license restriction of the Special Edition. Download the Evaluation version of CodeWarrrior, which is fully-featured (no code size limit) for thirty days.

---Tom
0 项奖励
回复