Help for MPC5668G

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help for MPC5668G

1,482 Views
cany
Contributor I

İ will use Freescale MPC5668G cpu.

 

İ am trying to write code on codewarrior. İ have several questions about these platforms.

 

  • İ can not find any simulator for MPC5668 CPU. Please tell me if there are any simulator which I can use?

 

  • I am thinking to buy MPC5668G/E Evuluation Kit for our project. Is this kit contain programmer like multilink, shortly Will I need another device or software for  CPU, is this kit enough?

 

  • Are there simple code for MPC5668G ?
Labels (1)
0 Kudos
Reply
1 Reply

1,120 Views
stanish
NXP Employee
NXP Employee

Hello cany,

 

regarding to your questions:

 

  • CodeWarrior does not include an instruction simulator.  You can use 3-rd party tools e.g. (Multi by GreenHills, Trace32 by Lauterbach...) which includes instruction simulator feature
  • the Evaluation kit includes: Board + MCU,  PEMICRO USB multilik debug cable, and the evaluation version of CodeWarrior tool (~30 days without any codesize limitations then switched into Special Edition variant). So in case you would like to use unlimited version of CodeWarrior tool you will probably need to buy a CodeWarrior suite:  http://www.freescale.com/webapp/sps/site/taxonomy.jsp?code=CW_SUITES&tid=CWH
  • Regarding the CodeWarrior examples, you can possibly reuse some exisiting examples available in CodeWarrior Examples directory: "<CW for MPC55xx and MPC56xx 2.x>\(CodeWarrior_Examples)\" 

Hope this will help you.

 

Stanish

0 Kudos
Reply