Full Simulation Chip debug on MCF51QE microcontroller

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Full Simulation Chip debug on MCF51QE microcontroller

2,036件の閲覧回数
jreyes085
Contributor I
Hi, How can i do a simulation of the MCF51QE microcontroller without having the demoboard? Can i do this?

I only have two options to choose, the first one is "P&E multilink/cyclone pro" and the second one is the "SofTec coldfire". I don´t have the option that makes the "full chip simulation", this option is available on the 08 MCU version.

Can i do something about this? thanks!
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,245件の閲覧回数
jreyes085
Contributor I
i upgraded the CW'to the 6.2 version and now it works with the full simulation chip....
0 件の賞賛
返信