Full Simulation Chip debug on MCF51QE microcontroller

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Full Simulation Chip debug on MCF51QE microcontroller

2,022 次查看
jreyes085
Contributor I
Hi, How can i do a simulation of the MCF51QE microcontroller without having the demoboard? Can i do this?

I only have two options to choose, the first one is "P&E multilink/cyclone pro" and the second one is the "SofTec coldfire". I don´t have the option that makes the "full chip simulation", this option is available on the 08 MCU version.

Can i do something about this? thanks!
标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,231 次查看
jreyes085
Contributor I
i upgraded the CW'to the 6.2 version and now it works with the full simulation chip....
0 项奖励
回复