Flash programmer for MPC8548

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash programmer for MPC8548

4,907 Views
PaoloTreffilett
Contributor II
Hi all,
   I'm using a EP8548A board with the MPC8548E processor. I have a problem when I try to use the Flash Programmer (CodeWarrior 8.7) and my Ethernet PowerTAP. Using the default configuration file for MPC8548CDS_sram_flash.cfg I can erase and verify the flash (AMD am29lv641d) sectors but I cannot program them.

I think that I'm doing some errors in the configuration or I'm not using the correct configuration file, does anyone have any suggestions on how to program the flash with this kind of board?

Thank you,
Paolo



Message Edited by Paolo Treffiletti on 2007-07-12 10:22 AM
Labels (1)
0 Kudos
Reply
4 Replies

2,568 Views
IMX31
Contributor I
Hello Paolo,
 
Can you please send the pdf schematics of MPC8548A.
 
Regards
Raghu
 
0 Kudos
Reply

2,568 Views
Voxan
Contributor III
Hi Paolo,

from the flash programmer UI:
1- press the load settings button.
2- pick 8548_CDS_sram_FlashBank#0.xml in the 85xx folder.
3- make sure the right connection, config file are selected
4- check the right flash device is selected in the next page.
5- than erase and blank check

Now create a dummy project from CW stationery wizard for 8548CDS
1- change build target from DEBUG to ROM
2- build the application

from 4th page of flash programmer:
1- select the binary you've just created with CW
2- set the format to binary/row
3- program
4- verify

does that help?

Best Regards

0 Kudos
Reply

2,568 Views
PaoloTreffilett
Contributor II
Thank you for your suggestion.

The problem is that I have already build a binary image with an external tool-chain (I mean, I have a u-boot.bin binary) and I need to place it in flash at the location 0xFFF80000 but with the Ethernet PowerTAP and the Flash Programmer (CW 8.7) I'm not able (until now, I hope :smileyhappy: ) to program these flash sectors.

With standard Embedded Planet 8548 boards I can write the flash using the u-boot already provided by EP (boards are shipped with a pre-installed u-boot), but this particular board has blank flash.

Paolo
0 Kudos
Reply

2,568 Views
Voxan
Contributor III
Paolo,

understood, the aim of the dummy project was to make sure the flash program was fine. The flash programmer refusing to flash may be due a ill formed .bin file.

I the suggestion does not do the trick than please log a bug at

http://www.freescale.com/webapp/sps/site/homepage.jsp?nodeId=054670&tid=FSH

press the "Submit a service request" link...

Regards
0 Kudos
Reply