Flash Programmer do not work after CW7.2 for coldfire update (works with 7.1)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash Programmer do not work after CW7.2 for coldfire update (works with 7.1)

2,173 Views
TomLEE
Contributor III

Hello,

I use USB-ML-CFE Rev.C from PE Micro for programming my aplication with CodeWarrior 7.1 on a MCF52230 coldfire.

It's works fine month ago.

But since I've updated with new 7.2 version, on the status window, when I tried to erase flash memory, there is: "Error: initialization failed."

 

Someone have an idea to help me ?

I don't know what to do !!!

 

Thank you for help,

Thomas.

Labels (1)
0 Kudos
Reply
2 Replies

1,506 Views
PunKidd
Contributor I

I'm getting the same failure with Code Warrior 7.2 using USB-ML-CFE rev. C.  Trying to connect to a M52235EVB board. 

I can make the project in CW and then flash it to the target with P&E's PROGCFZ starter addition and everyhing runs fine on the board, but I can't get it to connect/flash directly from CW. 

 

Any input on things to try would be welcome. 

0 Kudos
Reply

1,506 Views
aafreyre
Contributor I

Hi,

     I have the same problem, but my firmware is the revicion "D".

Is any sugestion out there?

Thank you Ariel

 

0 Kudos
Reply