FMPLLMPC5554 CW2.7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FMPLLMPC5554 CW2.7

1,965件の閲覧回数
khurram712
Contributor I

MPC5554 cook book includes a project that uses FMPLL.In the initialization source code,there is a loop in which there is  check for "LOCK" bit of "FMPLL.SYNSR" register as the main condition.The bit never sets to 1 and so the loop never ends.

Do i need to make some change in source code in order for PLL to occur or do i need to do something else in order to execute it properly.

 

Regards

 

Khurram Hameed

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,513件の閲覧回数
khurram712
Contributor I

can some one please answer this query...it straight out of the book code..still it is not working...any suggestion or solution...

0 件の賞賛
返信

1,513件の閲覧回数
stanish
NXP Employee
NXP Employee

Hi khurram712,

 

I've just tested FMPLL example and seems to work correctly with EVB MPC5554DEMO.

Do you use a custom board or Freescale EVB?

The example expects 8Mhz external crystal. What crystal do you have?

 

Stanish

 

0 件の賞賛
返信