Error installing USB drivers for CodeWarrior Probes. Both the initial install and the manual process fail. This is on Windows 7.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Error installing USB drivers for CodeWarrior Probes. Both the initial install and the manual process fail. This is on Windows 7.

1,267件の閲覧回数
jamesros
Contributor I


I was trying to install "CodeWarrior for PowerArchitecture (Eclipse-Windows Hosted) v10.4.exe"
I am running on Windows 7.

The install was run as administrator.

I have tried it several times.

The status on the Installation Wizard just says "Install failed" Is there any way to get more information?

ラベル(1)
0 件の賞賛
返信
1 返信

1,066件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello James Ros,

Is this error of CodeWarrior installation error or USB driver installation error?

Did you follow the steps in the driver read me file:

C:\Freescale\CW_PA_v10.4.0\PA\ccs\drivers\usb\readme.txt

Regards

Lunmin

0 件の賞賛
返信