Error Undefined InitializeUART

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Error Undefined InitializeUART

3,474 次查看
niravj
Contributor I

Hi,

 

I am using 53359evb along with mqx and Code warrior in my project.

 

After compiling the source code thoroughly there are few errors coming up

 

Error   : Undefined : "InitializeUART"
uart_console_io_cf.c line 42   Referenced from "__init_uart_console" in

Error   : Undefined : "ReadUARTN"
uart_console_io_cf.c line 80   Referenced from "__read_console" in

Error   : Undefined : "WriteUARTN"
uart_console_io_cf.c line 107   Referenced from "__write_console" in

Error   : Undefined : "__FLASHX_END_ADDR"
flash_mcf52xx.c line 82   Referenced from "mcf52xx_internal_flash_install" in

Error   : Undefined : "__FLASHX_SECT_SIZE"
flash_mcf52xx.c line 72   Referenced from "mcf52xx_internal_flash_install" in

Error   : Undefined : "__FLASHX_START_ADDR"
flash_mcf52xx.c line 96   Referenced from "mcf52xx_internal_flash_install" in

Error   : Undefined : "__VECTOR_TABLE_ROM_START"
vectors.c line 353   Referenced from "__boot" in

Error   : Undefined : "__VECTOR_TABLE_ROM_START"
init_bsp.c line 85   Referenced from "_bsp_enable_card" in

Error   : Undefined : "__VECTOR_TABLE_ROM_START"
Referenced from "_psp_saved_vbr" in

Link failed.

 

What are the library files i missed to add in system path/access path - any guidance will be greatly helpful...

 

Nirav

标签 (1)
标记 (1)
0 项奖励
回复
1 回复

1,830 次查看
niravj
Contributor I

It seems that I found answer to this problem..

 

My code was initially compiled by MQX 3.0 and Code Warrior 7.1.

 

Compiling the same code with MQX.3.4 or later and code Warrior 7.1 or 7.2 was giving this problem.

 

Nirav

 

0 项奖励
回复