Environment     Winddow XP        CW Power Architecture 8...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Environment     Winddow XP        CW Power Architecture 8...

2,751 Views
kaboo
Contributor I
Environment
    Winddow XP   
    CW Power Architecture 8.7
Hardware
    MPC 8349EA
    USB TAP
Set up
    Init file in attachment
    Target mem   0x007FF000
    Size               0x00006000
    Flash S29GL256N   16Mx16x1 base @ 0xF8000000
Try to do
    blank check
            FAILED
 
 
: -------------------------
Using utility file: FlashUtility.elf

======================================================================
=== Target Configuration Settings
=== Connection:    CodeWarrior USB TAP
=== Target Processor: 8349
=== Target Init File: E:\work\bootloader\8349ITX_init.cfg
======================================================================
Connecting......Connected

======================================================================
=== Execute: Blank Check
=== Timestamp:  Thu Jan  3 19:45:27 2008
=== Flash Device:   S29GL256N
=== Flash Organization:   16Mx16x1
=== Flash Mem Start Addr: 0xFE000000
=== Flash Mem End Addr:   0xFFFFFFFF
======================================================================
Informing other connection clients that the target is being 'clobbered'.
Loading Flash Utility Driver at: 0x00000000
Flash Programmer: Flash Programmer plugin failed to load the flash utility driver. The    magic number read from target memory after the image was loaded is incorrect.
Flash Programmer: Flash Programmer plugin failed to load the flash utility driver. The    magic number read from target memory after the image was loaded is incorrect.
Timestamp:  Thu Jan  3 19:45:27 2008
 
 
###################
i use DDR2 memory in my board. but the module of init file i used is design for DDR. i want to know how can i modify this module to initialize the DDR2 controller?
who have init file which include the DDR2 module? my email address is [email protected].
thank you for your help!!
Labels (1)
0 Kudos
Reply
1 Reply

1,244 Views
Voxan
Contributor III
Hi there and Happy new year 2008!!

I would recommand to contact the support line with the details about your DDR2 RAM...
They will contact the engineering team to get you a proper answer...

Support line is here:

http://www.freescale.com/webapp/sps/site/homepage.jsp?nodeId=05

click the 'Request Help (online)' link...

Hope this helps
Regards
0 Kudos
Reply