ECC_DETECT ACE error bit enabled after DDR initialization

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ECC_DETECT ACE error bit enabled after DDR initialization

1,525 Views
Em31
Contributor II

During the DDR initial enable of the A009803_Erratum process, the ACE bit of the ERR_DECTECT (0xE40) was triggered.

// 3. Set DDR_SDRAM_CFG[MEM_EN]
WRITE32(DDRmc1_SDRAM_CFG_ADDR, (DDRmc1_SDRAM_CFG_VAL | SDRAM_CFG_MEM_EN_MASK));

Can you explain why and what could cause the ACE bit to be triggered?
Also, we are wondering if ACE bit triggering will prevent the QCVS DDR validation process from being completed.

0 Kudos
Reply
1 Reply

1,483 Views
yipingwang
NXP TechSupport
NXP TechSupport

the ACE bit can be set when there is an HW issue or when the register setting is not optimized (most cases an incorrect combination of wrlvl_start, clk_adjust, odt, and driver setting can cause the ACE bit to be set).

First we need to make sure the DDR register settings are optimal (with good margins). this can be done using the QCS DDRv tool. Take a good working board and run the DDRv tool to optimize the register setting. then apply the optimized setting to the failing board.

0 Kudos
Reply