Driver visibility under XP virtual Machine

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Driver visibility under XP virtual Machine

ソリューションへジャンプ
3,633件の閲覧回数
punkinsmasher
Contributor I

I have just acquired a tower and am trying to run the demos. I have a 64 bit machine running Win 7 and have opened an XP Virtual machine under Windows Virtual PC.

 

The unvirtual side sees the USB cable and loads the LibUSB-Win32 Devices driver. CodeWarrior on the virtual side does not see the driver and so I can not erase/program flash.

 

Similarly, I have a USB to serial cable for the serial connection to the tower. The unvirtual side loads the driver and assigns it to COM5. The virtual machine is not even aware of the new com port.

 

Being new to virtual machines, can anyone direct me as to how these device drivers on the real machine can be seen on the virtual?

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,486件の閲覧回数
kef
Specialist I

I didn't try it on x64 windows, but "Windows XP Mode"-virtual machine on x86 Windows 7 is just fine with USB devices. Every time you attach USB device,  you should click on it in USB drop down menu in XP Mode window. This will attach USB device to XP. Doing this first time will make XP asking for XP drivers. At least USB<->serial converters are working fine.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,486件の閲覧回数
vier_kuifjes
Senior Contributor I

You can't access hardware devices like USB ports using Microsoft Virtual PC (I had this problem myself once). It should work with VMWare though...

0 件の賞賛
返信
2,487件の閲覧回数
kef
Specialist I

I didn't try it on x64 windows, but "Windows XP Mode"-virtual machine on x86 Windows 7 is just fine with USB devices. Every time you attach USB device,  you should click on it in USB drop down menu in XP Mode window. This will attach USB device to XP. Doing this first time will make XP asking for XP drivers. At least USB<->serial converters are working fine.

0 件の賞賛
返信
2,486件の閲覧回数
vier_kuifjes
Senior Contributor I

I didn't know this was possible in Windows 7 XP-mode. In a "regular" MS virtual PC environment this isn't possible.

0 件の賞賛
返信