Debugging the LX2160A using gdb/ gdbproxy

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debugging the LX2160A using gdb/ gdbproxy

1,871 次查看
Stephen_Williams
Contributor I

I'm looking to debug a LX2160A based target using the CodeWarrior TAP.

Our development environment is outside of the CodeWarrior ecosystem so i'm looking to perform the debugging without the CodeWarrior tool-chain.

The CW TAP contains a "GDB Proxy" to provide this capability, however we require some assistance in correctly configuring gdb and some examples of their use.

The document CWTAP_GDB_GSG (https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/cw-development-tools/6439/1/CWTAP_GDB_GS...) provides some information on how this is performed and states that NXP has an XML transformation script to convert the CodeWarrior target configurations into the required GDB format, however the link to the location of those configurations is dead.

Would it be possible to either provide the transformation script, a GDB configuration script for the LX2160A, or at least some example GDB configuration scripts for other targets (ideally with an example of usage) to use as a starting point?

Thanks for your help,
Stephen

0 项奖励
回复
1 回复

1,829 次查看
yipingwang
NXP TechSupport
NXP TechSupport

We only have gdb script for PowerPC platforms, no such scripts for Layerscape platforms.

 

Please refer to https://www.nxp.com.cn/docs/en/application-note/AN12270.pdf

0 项奖励
回复