Debugging the LX2160A using gdb/ gdbproxy

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugging the LX2160A using gdb/ gdbproxy

1,813件の閲覧回数
Stephen_Williams
Contributor I

I'm looking to debug a LX2160A based target using the CodeWarrior TAP.

Our development environment is outside of the CodeWarrior ecosystem so i'm looking to perform the debugging without the CodeWarrior tool-chain.

The CW TAP contains a "GDB Proxy" to provide this capability, however we require some assistance in correctly configuring gdb and some examples of their use.

The document CWTAP_GDB_GSG (https://community.nxp.com/pwmxy87654/attachments/pwmxy87654/cw-development-tools/6439/1/CWTAP_GDB_GS...) provides some information on how this is performed and states that NXP has an XML transformation script to convert the CodeWarrior target configurations into the required GDB format, however the link to the location of those configurations is dead.

Would it be possible to either provide the transformation script, a GDB configuration script for the LX2160A, or at least some example GDB configuration scripts for other targets (ideally with an example of usage) to use as a starting point?

Thanks for your help,
Stephen

0 件の賞賛
返信
1 返信

1,771件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

We only have gdb script for PowerPC platforms, no such scripts for Layerscape platforms.

 

Please refer to https://www.nxp.com.cn/docs/en/application-note/AN12270.pdf

0 件の賞賛
返信