Debugger problems

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
4,075件の閲覧回数
ralu
Contributor III

Debuuging does not work any more for CW 7.1 on MCF52235, because it looks like tha only one interrupt source works.

 

I can put one breakpoint, but after stop i can not make any steps, becuase it lost conenction.

 

 

 

I do not know why, but it can be due to drivers on PC or drivers on Multilink, but how can is solve this issue?

 

EDIT

 

I have two Multilinks Here (rev C and rev D)  I also have two boards to test on. Uploading FW works fine, but debuuging lost connection after first breakpoint.

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
3,804件の閲覧回数
ralu
Contributor III

Issue was that due to use of some software from pe-micro debugger got impropper FW.

I got new FW for multilink FE from pe-micro support.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,804件の閲覧回数
FridgeFreezer
Senior Contributor I

Are you disabling the PST data pins / setting them to other functions?

/* Enable debug */ #ifdef DEBUG MCF_GPIO_PDDPAR = 0x0F; // PST/DDATA Pins enabled #else MCF_GPIO_PDDPAR = 0; // Disabed - reduces EMC #endif

 

3,804件の閲覧回数
alager
Contributor II

Is this in the BDM driver somewhere, or just in the code?

We have an issue where the BDM is setting MCF_GPIO_PDDPAR = 0x0F, and we don't want that.

We need to use the PST pins as gpio.

Thanks,

Aaron

0 件の賞賛
返信
3,805件の閲覧回数
ralu
Contributor III

Issue was that due to use of some software from pe-micro debugger got impropper FW.

I got new FW for multilink FE from pe-micro support.

0 件の賞賛
返信