Debugger problems

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Debugger problems

跳至解决方案
4,144 次查看
ralu
Contributor III

Debuuging does not work any more for CW 7.1 on MCF52235, because it looks like tha only one interrupt source works.

 

I can put one breakpoint, but after stop i can not make any steps, becuase it lost conenction.

 

 

 

I do not know why, but it can be due to drivers on PC or drivers on Multilink, but how can is solve this issue?

 

EDIT

 

I have two Multilinks Here (rev C and rev D)  I also have two boards to test on. Uploading FW works fine, but debuuging lost connection after first breakpoint.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
3,873 次查看
ralu
Contributor III

Issue was that due to use of some software from pe-micro debugger got impropper FW.

I got new FW for multilink FE from pe-micro support.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
3,873 次查看
FridgeFreezer
Senior Contributor I

Are you disabling the PST data pins / setting them to other functions?

/* Enable debug */ #ifdef DEBUG MCF_GPIO_PDDPAR = 0x0F; // PST/DDATA Pins enabled #else MCF_GPIO_PDDPAR = 0; // Disabed - reduces EMC #endif

 

3,873 次查看
alager
Contributor II

Is this in the BDM driver somewhere, or just in the code?

We have an issue where the BDM is setting MCF_GPIO_PDDPAR = 0x0F, and we don't want that.

We need to use the PST pins as gpio.

Thanks,

Aaron

0 项奖励
回复
3,874 次查看
ralu
Contributor III

Issue was that due to use of some software from pe-micro debugger got impropper FW.

I got new FW for multilink FE from pe-micro support.

0 项奖励
回复