Could not determine GDB version using command

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Could not determine GDB version using command

4,005 次查看
ts1234
Contributor III

I am observing the following error on debugging a bare-metal app on LS1043ARDB.

Could not determine GDB version using command: C:\Freescale\CW4NET_v2020.06\CW_ARMv8\ARMv8\gdb\bin\aarch64-fsl-gdb.exe --version

How do I fix this?

0 项奖励
回复
3 回复数

3,045 次查看
annlily
Contributor I

I would like to find out too – following.

 
0 项奖励
回复

4,000 次查看
yipingwang
NXP TechSupport
NXP TechSupport

I can get the version information as the following.

Microsoft Windows [Version 10.0.18363.2094]
(c) 2019 Microsoft Corporation. All rights reserved.

C:\Users\nxa22585>C:\Freescale\CW4NET_v2020.06\CW_ARMv8\ARMv8\gdb\bin\aarch64-fsl-gdb.exe --version
GNU gdb (GDB) 7.11.1.0.05c0cb628d-b200311 (NXP Semiconductors)
Copyright (C) 2016 Free Software Foundation, Inc.
License GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html>
This is free software: you are free to change and redistribute it.
There is NO WARRANTY, to the extent permitted by law. Type "show copying"
and "show warranty" for details.
This GDB was configured as "--host=i686-w64-mingw32 --target=aarch64-fsl-linux".
Type "show configuration" for configuration details.
For bug reporting instructions, please see:
<http://www.gnu.org/software/gdb/bugs/>.
Find the GDB manual and other documentation resources online at:
<http://www.gnu.org/software/gdb/documentation/>.
For help, type "help".
Type "apropos word" to search for commands related to "word".

C:\Users\nxa22585>

0 项奖励
回复

3,930 次查看
ashlidurden
Contributor I

I would like to find out too – following.

every daily wordle puzzle
0 项奖励
回复