Combining s19 files

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Combining s19 files

2,178件の閲覧回数
skyguy
Contributor III
Various older posts refer to a 'burner.exe' utility program and a 'hexfile' command in the CodeWarrior linker.  Neither of these seems to exist in the version of CodeWarrior I'm using (7.1, on Windows Vista).  Does anyone know what happened to these, or can anyone suggest an alternative tool?  I need to combine two programs into one production load file.
Thanks,
Rick
ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,143件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hello,

the burner is part of the CodeWarrior for S12 or for MCU (S08 and ColdFire V1).

I suggest you download the free special edition version from here:

http://www.freescale.com/lgfiles/devsuites/HC08/CW_MCU_V6_3_SE.exe?WT_TYPE=IDE%20-%20Debug,%20Compil...

 

The burner.exe is located in the prog folder.

 

BK

0 件の賞賛
返信