Coldfire TCP/IP Lite and Codewarrior 7.0

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Coldfire TCP/IP Lite and Codewarrior 7.0

4,007件の閲覧回数
vier_kuifjes
Senior Contributor I
In the documentation that comes with the Coldfire TCP/IP Lite version 2.0 there's a paragraph saying:

Code:
ColdFire TCP/IP Lite ProjectVersion 2.0 October 12, 2007
CodeWarrior for ColdFire currently has a stable release with Version 6.4.A Version 7.0 is expected in December 2007 and a new drop of this projectwill be released then. This is why we have included 6.4 in the filename.

But until today there's no sign of a newer, CW7.0 compatible version.

Any idea when this new version is to be expected?


Message Edited by Marc VDH on 2008-07-02 04:19 PM
ラベル(1)
タグ(1)
0 件の賞賛
返信
4 返答(返信)

1,919件の閲覧回数
vier_kuifjes
Senior Contributor I
There must be someone who knows??
0 件の賞賛
返信

1,919件の閲覧回数
CrasyCat
Specialist III

Hello

CodeWarrior for Coldfire V7.1 is available for download on Freescale web page.

Go to http://www.freescale.com/CodeWarrior
Click on the link "ColdFire® Architectures (V2, V3, V4)  "
Click on the  "Downloads" Tab

If you wants to use a special edition software:
Then click on the button "Download next to "Special Edition: CodeWarrior for Coldfire Architectures  "

If you want to use an evaluation version
Then click on the button "Download next to "Evaluation for Coldfire Architectures  "

You will need to log in into the Freescale web to be able to download the software.
This evaluation version will come with a 30-days time limited key.

CrasyCat
0 件の賞賛
返信

1,919件の閲覧回数
allawtterb
Contributor IV
I don't think that is his issue.  He is wanting to know if there is a release of the TCP/IP Lite Project that works with v7.0/v7.1.
0 件の賞賛
返信

1,919件の閲覧回数
vier_kuifjes
Senior Contributor I
Actually it wasn't my issue, but in the mean time I found out that the most recent version of TCP/IP lite does compile and run nicely when compiled with CW7.0 or CW7.1

The additional bonus of CW7.1 is that it creates more compact code than CW7.0 does.
0 件の賞賛
返信